Remove and Install the Power Structure Fan Assembly - Frame 6L
Replace a power structure fan assembly with kit catalog number SK-RM-PSFAN1-F6L. Follow these steps to remove and install the power structure fan assembly.
- Review the product advisories in Before You Begin.
- Remove power from the system.
- IMPORTANT: The fan assembly power wire harness is connected inside the chassis. You cannot remove the fan assembly until you disconnect the fan power wire harness.
- Loosen the two M4 captive, Phillips® screws that secure the fan assembly to the chassis and pull the fan assembly away from the chassis to expose the fan power wire harness connector.
- Reach into the chassis and disconnect connector P42 from J42 and remove the fan assembly.
- Install the power structure fan assembly in the reverse order of removal.
Provide Feedback