Remove and Install the DR and PE-A (EMC and MOV) Jumper - Frame 6L
Replace the DR and PE-A (EMC and MOV) jumper with kit catalog number SK-RM-JMPR1-F6L. Follow these steps to remove and install the DR and PE-A (EMC and MOV) jumper.
- Review the product advisories in Before You Begin.
- Remove power from the system.
- Remove the cover from the chassis. See Remove and Install the Frame 6L Cover.
- Remove the fan power supply circuit board. See Remove and Install the Fan Power Supply Circuit Board - Frame 6L.
- Loosen the three M4 captive, slotted-Torx screws that secure the PE-A jumper to the power interface circuit board.
- Lift the jumper away from the power interface board until the keyholes in the jumper align with the pins on the sidewall and remove the jumper.
- TIP: This image shows a top view of the PE-A jumper (A) set to the default (IN) position.
- Install the DR and PE-A (EMC and MOV) jumper in the reverse order of removal.
- Verify that the jumper is installed in the correct position as required for your grounding scheme and application. See the PowerFlex 750-Series Products with TotalFORCE Control, Installation Instructions, publication 750-IN100, for jumper configuration.
Provide Feedback