Remove and Install the Stirring Fan Assembly for Frame 5
Replace a stirring fan assembly with kit catalog number SK-RM-MFAN1-F5. Follow these steps to remove and install the stirring fan assembly.
- Review the product advisories in Before You Begin.
- Remove power from the system.
- Remove the cover from the chassis. See Remove and Install the Frame 5 Cover.
- Disconnect the wire harness connector P12 from connector P1 on the fan assembly bracket.
- Loosen the two captive screws that secure the fan assembly to the chassis and remove the fan assembly.
- Install the stirring fan assembly in the reverse order of removal.
Provide Feedback