Remove and Install the Fan Power Supply Circuit Board for Frame 5
Replace a fan power supply circuit board with kit catalog number SK-RM-PSB1-F5-F6. Follow these steps to remove and install the fan power supply circuit board.
- Review the product advisories in Before You Begin.
- Remove power from the system.
- Remove the cover from the chassis. See Remove and Install the Frame 5 Cover.
- Disconnect these cable connectors from the fan power supply circuit board:
- P1 from J1
- P2 from J2
- Remove the six M4 x 10 mm Torx screws that secure the fan power supply circuit board to the bracket and remove the board.
- Install the fan power supply circuit board in the reverse order of removal.
Provide Feedback