Remove Power from the System for Frames 5, 6 and 6L
This procedure must be completed before attempting to service any part of a frame 5, 6, or 6L liquid cooled drive.
ATTENTION:
Risk of injury or equipment damage exists.
Remove power before you remove or make cable connections. When you remove or insert a cable connector with power applied, an electric arc can occur. An electric arc can cause personal injury or property damage in the following ways:
- An electric arc can send an erroneous signal to system field devices, which can cause unintended machine motion
- An electric arc can cause an explosion in a hazardous environment
Electric arcs cause excessive wear to contacts on both the module and its receiving connector. Worn contacts can create electrical resistance.
Follow these steps to remove power from a frame 5, 6 and 6L drive.
- Turn off and lock out all input power, including any external power sources.
- Wait 15 minutes.
- If present, remove the conduit box cover from the drive.
- To verify that there is no voltage present, measure the AC input and DC bus voltage:
- For AC input drives and bus supplies only, measure the AC input terminals R/L1, S/L2, and T/L3, L to L and L to chassis GND (PE).
- For frames 5 and 6 products, measure the DC output terminals; DC+ to DC–, DC+ to chassis GND (PE), and DC– to chassis GND (PE).
- For frame 6L, measure the DC bus voltage between the DC+ and DC– testpoint sockets on the bottom of the chassis. Also measure between the DC+ testpoint and the PE ground bus bar (GND) and the DC– testpoint and PE ground bus bar (GND).
Frame 5 Power Terminal Identification
Frame 6 Power Terminal Identification
Item | Name | Description |
---|---|---|
A | PE grounding stud | Termination point to chassis ground for AC line shield |
B | R/L1, S/L2, T/L3 | AC line input power terminals |
C | DC+, DC– | DC bus terminals |
D | U/T1, V/T2, W/T3 | AC output motor terminals |
E | PE grounding stud | Termination point to chassis ground for motor shield |
Frame 6L Power Terminal Identification
Item | Name | Description |
---|---|---|
A | PE grounding bus | Termination point to chassis ground |
B | R/L1, S/L2, T/L3 | AC line input power terminals |
C | U/T1, V/T2, W/T3 | AC output motor terminals |
D | DC+, DC– | DC bus testpoint sockets |
Provide Feedback