Hardware Installation Diagrams

The assembly illustrations throughout this manual contain diagrams (as shown here) that identify the following: sequence number (if necessary), type of fastener, fastener size, tool type and size, and final assembly torque.
Fastener Diagram
Image with callouts of the fastener diagram that describes fastener type, size, tool, and final torque.
Fastener Diagram Elements
Item
Name
Description
A
Sequence number
The sequence number corresponds with a step in a procedure.
B
Fastener type
A graphic representation of the fastener drive type.
C
Fastener size
Specifies diameter x thread pitch x length as necessary.
D
Tool type and size
The recommended tool for the specified drive type.
E
Torque
Specifies the final assembly torque for the fastener.
Fastener Drive Types
Image of a flat-head screw drive head.
Flat-head screw
Image of a Hexagonal bolt drive head.
Hexagonal bolt
Image of a Hexagonal nut drive head.
Hexagonal nut or standoff
Image of a Hexagonal screw drive head.
Hexagonal screw
Image of a Torx screw drive head.
Torx screw
Image of a Phillips screw drive head.
Phillips screw
Image of a Pozidriv screw drive head.
Pozidriv screw
Image of a Slotted torx screw drive head.
Slotted torx screw
Image of a Slotted Phillips screw drive head.
Slotted Phillips
Tool Types
F
Flat-nose screwdriver
Px
Phillips screwdriver/bit and size
PZx
Pozidriv screwdriver/bit and size
Txx
Torx screwdriver/bit and size
xx mm
Hexagonal socket wrench
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal