Fiber Transceiver with XT Kit
Use the fiber transceiver with XT kit, catalog number SK-RM-FTR1-F8-XT, to replace a contaminated or corroded transceiver. The transceiver with XT contains dielectric grease on the edge connector. Do not remove the protective covers before installation.

Fiber Transceiver with XT Kit Contents
Item | Description |
---|---|
A | Fiber transceiver with XT |
B | Electrostatic discharge (ESD) strap |
Provide Feedback