Metal Form Instructions
    | AVC | Name | Description | 
|---|---|---|
| AVC | Auxiliary Valve Control | Controls an auxiliary valve that is used with a main valve. | 
| CBIM | Clutch Brake Inch Mode | Used for press applications where minor slide adjustments are required, such as press setup. | 
| CBCM | Clutch Brake Continuous Mode | Used for press applications where continuous operation is desired. | 
| CBSSM | Clutch Brake Single Stoke Mode | Used in single-cycle press applications. | 
| CPM | Crankshaft Position Monitor | Used to determine the slide position of the press. | 
| CSM | Camshaft Monitor | Monitors motion for the start, stop, and run operations of a camshaft. | 
| EPMS | Eight-position Mode Selector | Monitors eight safety inputs to control one of the eight outputs that correspond to the active input. | 
| MMVC | Maintenance Manual Valve Control | Used to drive a valve manually during maintenance operations. | 
| MVC | Main Valve Control | Controls and monitors a main valve. | 
Provide Feedback