Safety Application Instructions
    Safety application instructions are certified for use in SIL 2 or SIL 3 applications.
     ATTENTION: 
    
Safety application instructions are the only instructions that can be used in the safety task for SIL 2 or SIL 3 applications.
For more information about using instructions, see the following:
- Logix 5000 Safety Application Instruction Set Reference Manual, publication 1756-RM095
- Logix 5000 Controllers General Instructions Reference Manual, publication 1756-RM003
Provide Feedback