Input Points View
Input Points is only available if you choose This Controller for the Configured By
parameter on the Module Definition dialog.
You must configure each point to use it in a safety application. The inputs are disabled
by default.
Input Points View Example

For more information on input delay times, see Safety Input Delay Time.
Ptxx Diagnostics
To view the Ptxx diagnostics, select Diagnostics in the Input Points view.
Ptxx Diagnostics Example

Provide Feedback