Chxx View
The Chxx view, where xx represents the channel number, shows the configuration options
available for the respective channel.
You can do the following actions on this view:
- Disable the channel, if desired
- Change the input type
- Set the notch filter
- Enable or disable open wire detection
- Set the scaling and recalculate all configurations with engineering unit
- Set digital filter
- View channel diagnostics information
TIP:
To latch and configure alarm parameters, go to
Alarms view.
Chxx View Example

Recalculate Units
Recalculate Units lets you recalculate all configurations with engineering unit after
a scaling change. Consider the following:
- The Recalculate Units option is enabled when the scaling configuration is changed.
- Upon selecting Recalculate Units option, the recalculated new values based on the new scaling configuration are displayed together with the old values for you to verify before changing.
- If you select "Yes" to proceed with the change, the new values will be set but it gets applied when you select "Apply/OK".
- If you select "No" to cancel the change, the old values are retained. You can either select the Recalculate Units again or manually change those configurations based on the new scaling.

Provide Feedback