Channels View

The Channels view shows an overview of the configuration values for all module channels.
TIP: Not all channel configurations are included in Channels view. To view or change the complete set of the channel configuration and also to view the diagnostics information for the channel, use Chxx view.
You can do the following actions on this view for all the channels:
  • Disable the channel, if desired
  • Change the input type
  • Set the notch filter
  • Enable or disable open wire detection
  • Set the scaling and recalculate all configurations with engineering unit
  • Set digital filter
  • Disable alarms
Channels View Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal