Generic ASCII Transmit View
    Use Generic ASCII Transmit view to configure parameters for transmitting ASCII data
            through serial module.
Generic ASCII Transmit View Example

| Parameter | Definition | Available Choices | 
|---|---|---|
| Swap Mode | Determines how the data that is transmitted to the Serial port is
                                    arranged. The swap is performed before the module sends output
                                    data. | 
 
     TIP: 
    A, B, C, and D represent
                                        four adjacent bytes in the received/transmitted data. | 
| Termination Mode | Determines the usage of the Termination Delimiters in the
                                    data. | 
 
     TIP: 
    The End Delimiter is only
                                        applied when the tag OxASCII.TxDataLength is set to 0. When
                                        the Ox.ASCII.TxDataLength is greater than 0, the effective
                                        Termination Mode is Ignore End Delimiter. | 
| Termination Delimiter 1 | Specifies the channel's first Termination Delimiter. The
                                    Termination Delimiter is used to signal the end of the data.
                                 | 
 | 
| Termination Delimiter 2 | Specifies the channel's second Termination Delimiter. | 
 If you enter $, it means that the Termination Delimiter 2 is not
                                    used. | 
| Diagnostics | When the controller status is online, open the Diagnostics dialog
                                    to view the diagnostic counters for performance and error
                                    management with the Generic ASCII communication. | – | 
Select Diagnostics to see the diagnostic information of the Generic ASCII
            Transmit/Receive channel.
Generic ASCII Transmit/Receive Channel Diagnostics

Provide Feedback