Connection View
    Use Connection to define controller-to-device behavior. 
- Set the RPI rate. For more information, see Requested Packet Interval.
- Select Unicast or Multicast connection to use on the EtherNet/IP network. For more information, see Unicast or Multicast Connection.
- View the reason for a connection fault.TIP:If there is a connection fault, the Connection Fault area displays the error code with a description that helps you to troubleshoot the module. For more information, see Troubleshoot Your Module.
- Inhibit the module. For more information, see Module Inhibiting.
- Configure whether a connection failure while the controller is in Run mode causes a major or minor fault.
- Enable or disable Automatic Diagnostics.ATTENTION:If you do not enable Automatic Diagnostics, the device does not publish diagnostics to FatoryTalk Alarms and Events.
Connection View Example

Provide Feedback