Safety Application Suitability Levels
    | Suitability Level | Conditions | Notes | 
|---|---|---|
| Applications that are rated up to, and including, SIL 2 as
                                    defined in IEC 61508, and PLc, Cat. 2 as defined in ISO
                                    13849-1 | The modules uses single-channel mode: 
 | Consider the following: 
 The larger safety system within which the safety I/O module
                                    resides can provide the diagnostics necessary to achieve the
                                    stated Suitability Level without the requirement that Point mode
                                    be Safety Pulse Test. To achieve the specific Safety Integrity Level, see the wiring
                                    diagrams for the respective safety module. | 
| Applications that are rated up to, and including, SIL 3 as
                                    defined in IEC 61508, and PLe, Cat. 4 as defined in ISO
                                    13849-1 | The modules use single-channel mode: 
 The modules use dual-channel mode: 
 The modules use dual-channel mode: 
 | 
Provide Feedback