Runtime and firmware update

Software updates for HMIs and IPCs, or routers are related to the operating system running on each device. A Runtime or a firmware update may be required to use the HMI or iPC.
Operating System and device
Software update
ASEM 6300 iPCs and third-party devices with Windows Runtime
Runtime
Stratix® 4300
, OptixPanel, Embedded Edge Compute Module and OptixEdge
Firmware (Runtime, System Manager, OS image, FactoryTalk Optix)
You can update your device Runtime and firmware in two ways:
NOTE: The updating process may require automatically restarting a remote device. Before planning any software or firmware update, make sure that the plant machinery is properly secured.

Manual Runtime and firmware update

  1. In
    FactoryTalk® Remote Access
    Manager, access the
    Tools
    Download
    section.
  2. Select
    Download
    next to the desired update. You will be directed to a specific Rockwell Automation webpage. Once your request will be authorized, you will receive an email including a link for the actual update download.
  3. Download the install file and store it on your device.
  4. Depending on your device:
    • If you are updating Windows Runtime for ASEM 6300 iPCs or third-party devices, run the install file to proceed with the Windows Runtime update.
    • If you are updating Ubuntu 22 Runtime for ASEM 6300 iPCs or third-party devices, see Ubuntu 22 Runtime installation and configuration.
NOTE: Make sure that your device is not restarted while the update is in progress.

Over-the-air (OTA) update

Access
FactoryTalk® Remote Access
Manager to run or schedule automatic updates for your device:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal