Which ports and public IPs shall I allow through my company firewall?
TCP protocol
To enable the communication service between the Internet protocol and the , at least one of the following TCP
ports of the remote services shall be set to open on the main servers of the Server
Infrastructure. The ports listed below are set as default and can be accessed and viewed
through the computer settings.
FactoryTalk®
Remote Access™
Manager- 80
- 443
- 5935
Furthermore, both the Runtime and router need to resolve the Infrastructure servers IP address through a dedicated domain name resolution server (DNS). To enable this process, the following ports shall be set to open:
- TCP 53
- UDP 53
The connection from clients to the Access Server uses TLS 1.2 with certificate
authentication. Clients can use the default TCP 443 outgoing port or can be configured to
use port 80 or 5935 (TLS is still in use), depending on which solution is best to comply
with local IT policies. Clients automatically test available outgoing ports, but they can be
configured to operate with a fixed port.
NOTE:
Access Servers are redundant and fault
tolerant.
NOTE:
FactoryTalk®
Remote Access™
Tools and Runtime need to be able to connect to
the following addresses: Access server:
- accessserver.cloud.rockwellautomation.com
Relay servers:
- ubiquityrs1.asem.it (Germany)
- ubiquityrs2.asem.it (Italy)
- ubiquityrs3.asem.it (USA - West Coast)
- ubiquityrs4.asem.it (USA - East Coast)
- ubiquityrs5.asem.it (Singapore)
- ubiquityrs6.asem.it (Hong Kong)
- ubiquityrs7.asem.it (Brazil)
- ubiquityrs8.asem.it (USA - South Central)
- ubiquityrs9.asem.it (USA - North Central)
- ubiquityrs10.asem.it (Central India)
- ubiquityrs11.asem.it (Central Australia)
- ubiquityrs12.asem.it (Italy)
Platform server:
- ftra-webapi.cloud.rockwellautomation.com
While a VPN connection is being established, the
FactoryTalk®
Remote Access™
Tools and Runtime perform a check to determine
the duration it takes for data to reach each Relay Server. This information assists the
Access Server in selecting the most optimal Relay Server to be utilized, regardless of
the geographical location of the device.Remote devices and the router then search for any open port to establish a server connection and consequently an end-to-end connection.
These settings allow you to locate each device by its own IP address within the network
through the Tools.
FactoryTalk®
Remote Access™
NOTE:
See FactoryTalk Remote Access Manager Tools for further information on this
subject.
SSL/TLS protocol
All of the connections available in the are made through an SSL/TLS
protocol, regardless of the port used for each connection. This protocol allows for a safe
and private data transaction between the server and Runtime.
FactoryTalk®
Remote Access™
Manager
NOTE:
Access Servers use an SSL server certificate signed by a Certification Authority (CA) to authenticate content transferred through web servers.
SNTP protocol
The UDP 123 port shall be set to
open
, to allow the clock synchronization through the SNTP protocol.Provide Feedback