Supported Libraries in FactoryTalk Optix

FactoryTalk® Optix
supports libraries that ease application development with predefined faceplates, devices, and objects.
The following libraries are supported:
  • Power Device Library - For more information, see publication DEVICE-RM100
  • Safety Device Library - For more information, see publication DEVICE-RM005
  • Plex APM Library - For more information, see publication INFO-RM005
  • Plex QMS Library - For more information, see publication INFO-RM006
  • Fiix Library - For more information, see publication INFO-RM007
You can download the libraries at the Product Compatibility and Download Center (PCDC). The PCDC is available at: rok.auto/pcdc.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal