Runtime launch
If you start your application as a service, Runtime launches automatically, without the need
for a user to log in. In this case, you cannot use a Native Presentation Engine. The Runtime
will work regardless of whether you have a user interface, for example, in the case of a
gateway.
TIP:
See
Configure a presentation engine
in the FactoryTalk® Optix™
online Help.If your application does not run as a service, you must login to allow Runtime to launch.
- Once you have installed the Runtime Tools, clickConfigureto launch them and selectRun FactoryTalk Optix as a service.
- Deploy application to the target device.TIP: See Deploy a FactoryTalk Optix Application.
Provide Feedback