Deploy a FactoryTalk Optix Application
Rockwell Automation
target devices automatically run FactoryTalk Optix Applications
upon deployment. Devices that do not have the update service installed or have the runtime application transferred manually require you to start the application manually on the device or configure the application for automatic startup. Use
FactoryTalk Optix Studio desktop editor
to deploy to either local or remote devices. Use FactoryTalk Optix Studio web editor
to deploy to remote devices only. FactoryTalk Optix Studio
uses FactoryTalk Remote Access
to deploy to remote devices.
IMPORTANT:
If a
FactoryTalk Optix Application
is already running on a target device, deploying another FactoryTalk Optix Application
stops and removes the other application.Prerequisites
- (optional) Configure the presentation engine for the mode in which you will be runningFactoryTalk Optix.
- Confirm thatFactoryTalk Optix Application Update Serviceruns on the target device.IMPORTANT: To operate correctly when running as an application,FactoryTalk Optix Application Update Servicerequires the TCP port 49100 to be reachable and a valid username with a configured password.
- Confirm that the target device has a valid license.IMPORTANT: If the target device is not licensed,FactoryTalk Optix Applicationsrun in the demo mode and stop automatically after 2 hours.
- Configure a device.IMPORTANT: Configure either a local or remote device. To configure a local device, see Manage target devices. To configure a remote device, openFactoryTalk® Hub™and accessFactoryTalk Remote Access. In FactoryTalk Remote Access Online Help, seeDomain viewand scroll toTo add a device. The remote device must also have theFactoryTalk Remote AccessRuntime client installed and configured. In FactoryTalk Remote Access Online Help, seeClient configuration.
- To deploy aFactoryTalk Optix Application
- Select the configured device.For more information, see Select a target device.
- If you selected a remote device, you must first establish a VPN connection to that device. Selector a remote desktop connection by selectingVPN.Remote Desktop
- Select.Run
- Enter the user password for the target device and selectOK.TIP: If you deploy a project to a target device where a project with the same name is already running, you are prompted toUpdateorReplacethe project at runtime.
- Updateoverrides the runtime project elements, but retains application files on the device.
- Replaceoverrides all runtime project and application files that were present on the device. Replaced application files cannot be recovered.
- To detachFactoryTalk Optix Studiofrom the target device, closeOutput.
- To stop theFactoryTalk Optix Applicationon the target device, select.StopTIP:If you uninstall Runtime Tools, the next time you log in, your application will automatically restart. You cannot deploy an application after Runtime Tools are uninstalled because the uninstall removes the update service.
The application on the target device stops.
TIP:
To detach
FactoryTalk Optix Studio from the target deice, close the Output pane in
FactoryTalk Optix
. The application continues to run on the target device but FactoryTalk Optix
is no longer connected so messages no longer appear in the Output
pane.deploy
Provide Feedback