Create a constrained variable

Create a variable with high and low value limits that will be linked with the gauges.
  1. In
    Project view
    , right-click
    Model
    and select
    New
    Variable
    .
  2. Hover-over the variable, select
    Edit
    , and enter
    ConstrainedVariable
    .
  3. In
    Properties
    , set
    ConstrainedVariable (Int32)
    to
    30
    .
  4. Right-click
    ConstrainedVariable
    and select
    New
    Range
    .
  5. Under
    EURange
    , set the properties:
    1. Set
      Constraint
      to
      True
      .
    2. Set
      High limit
      to
      50
      .
    3. Set
      Low limit
      to
      20
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal