Develop a constrained linear gauge
Develop an interface that enables you to change the current value, max value, and minimum value of a variable.

NOTE:
Download a sample project:
ConstrainedLinearGauge.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.

Select
to run the project using the client
emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback