Create a NetLogic to modify the image

Prerequisites
Set the default external code editor. See Set the default code editor.
  1. To create the NetLogic to hide the image
  2. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Runtime NetLogic
    .
  3. Double-click the NetLogic.
    The external code editor opens.
  4. Edit the NetLogic by replacing it with the following code. See Edit a NetLogic.
    #region Using directives using System; using UAManagedCore; using OpcUa = UAManagedCore.OpcUa; using FTOptix.HMIProject; using FTOptix.Retentivity; using FTOptix.UI; using FTOptix.NativeUI; using FTOptix.CoreBase; using FTOptix.Core; using FTOptix.NetLogic; #endregion public class RuntimeNetLogic1 : BaseNetLogic { public override void Start() { // Insert code to be executed when the user-defined logic starts } public override void Stop() { // Insert code to be executed when the user-defined logic is stopped } [ExportMethod] public void replaceSVG() { // LogicObject.Owner is the button, so LogicObject.Owner is the MainWindow AdvancedSVGImage svgImage = LogicObject.Owner.Get<AdvancedSVGImage>("AdvancedSVGImage1"); string myXML = "<?xml version=\"1.0\" encoding=\"iso-8859-1\"?>\r\n<svg version=\"1.1\" id=\"Overall\" xmlns=\"http://www.w3.org/2000/svg\" xmlns:xlink=\"http://www.w3.org/1999/xlink\" xml:space=\"preserve\" viewBox=\"0 0 300 300\">\r\n <g id=\"Box1\">\r\n <polygon style=\"fill:#CB8252;\" points=\"25,270 75,270 75,220 25,220\" transform=\"rotate(0, 20, 20)\"/>\r\n </g>\r\n</svg>\r\n"; //Update the SVG svgImage.SetImageContent(myXML); } }
  5. Save the code.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal