Develop a button that replaces an SVG image
Create a button and NetLogic that modifies an SVG image at runtime.
NOTE:
Download a sample project:
ReplaceImage.zipApplication example

Prerequisites
- To develop the project
- Arrange the interface elements.

Select
to run the project using the client
emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback