Create application logic

Create a dynamic link between the label and either the ClockLogic or System object.
  1. In
    Project view
    , select
    DateTimeLabel
    .
  2. In
    Properties
    , create a dynamic link between
    Text
    and either:
    • ProjectName
      NetLogic
      ClockLogic
      Time
      .
    • ProjectName
      NetLogic
      ClockLogic
      UTCTime
      .
    • ProjectName
      System
      System
      Date and time
      Date time
      .
    For more information about dynamic links, see Create dynamic links.
    TIP:
    While creating the dynamic link, use
    Format
    to select a different date and time format.
    If you get time from ClockLogic, you can expand the
    Time
    or
    UTCTime
    nodes to access
    Year
    ,
    Month
    ,
    Day
    ,
    Hour
    ,
    Minute
    , and
    Second
    variables.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal