Develop a label that displays the current date and time
Create a label and a dynamic link to a variable exposed by ClockLogic or System to display current date and time at runtime.
Application example

TIP:
You can download a sample project from:
DisplayCurrentDateTime.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select
to run the project using the client
emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback