Installation and system requirements FAQs
Where can I download FactoryTalk Optix Studio?
You can download FactoryTalk Optix Studio from FactoryTalk Hub. See FactoryTalk Optix Installation Guide |
FactoryTalk Optix Studio setup.
Is FactoryTalk Optix Studio free to download and use?
Yes, FactoryTalk Optix Studio is free to download and use. If you want to use all
available features, you need to buy FactoryTalk Optix Studio Pro. See FactoryTalk Optix Installation Guide |
FactoryTalk Optix Studio versus FactoryTalk Optix Studio Pro.
What are the system requirements for FactoryTalk Optix Studio and FactoryTalk
Optix Applications?
You can find system requirements for FactoryTalk Optix Studio and FactoryTalk Optix
Applications in the release notes. See FactoryTalk Optix Release Notes | System
requirements.
Which ports do I need to open for FactoryTalk Optix Studio and for a FactoryTalk
Optix Application?
You need to configure firewalls and ports to ensure successful between different
FactoryTalk Optix components. See Network ports configuration.
Where can I download Visual Studio® or Visual Studio Code® and check the
requirements?
Download the .NET Framework® and check the requirements on the Microsoft®
website.
Provide Feedback