Network ports configuration
Configure firewalls and ports to ensure successful communication. Review the default values for user-configurable ports and the comprehensive list of ports used by
FactoryTalk Optix
for inbound and outbound connections.
TIP:
Ports 80 and 443 may be already configured for devices like OptixPanels and Embedded Edge Compute Module (EECM).
FactoryTalk Optix modules
- WebPresentationEngine
- Protocol: This port is configurable. If Protocol is blank, the port reflects the protocol configuration.
- If set to HTTP: 80/TCP
- If set to HTTPS: 443/TCP
- ApplicationUpdateServer
- Fixed Port: 49100/TCP
- Communication Drivers
- RA Ethernet/IP Driver
- Port: 44818/TCP
- Modbus
- Port: 502/TCP
- Melsec FX3U: Configure the TCP port on PLC.
- Default port: 1034/TCP
- Melsec Q: Configure the TCP port on PLC.
- Default port: 1/TCP
- Omron Ethernet/IP
- Port: 44818/TCP
- Omron FINS
- Port: 9600/TCP
- S7 TCP
- Port: 102/TCP
- S7 TIA
- Port: 102/TCP
- TwinCAT
- Port: 851/TCP
- CODESYS
- Port: 1217/TCP
- DataStores
- SQL/SQL Express
- Port: 1433
- MySQL
- Port: 3306
- User Authentication
- LDAP: Configurable in the domain server address
- Default port 39.
- AD: This port is configurable. If AD is blank, the port reflects the protocol configuration.
- The default port is 39.
- OPC UA
- Server: User-configurable
- Default port: 59100/TCP
- Client
- The port depends on source server configuration.
- FTRA Service
- Ports: 5000/TCP, 14273/TCP, and 5936/TCP
- FT Hub
- FactoryTalk Optix acts as a client, using a random port at every connection.
External modules from TemplateLibrary
- MQTT (PushAgent and MQTTLogic):Configure these ports depending on the server configuration:
- Standard: 1883/TCP
- Secure: 8883/TCP
- Email (AlarmsWithEmailNotification):Configure these ports depending on the server configuration:
- SMTP
- 57/TCP, 25/TCP, or 465/TCP
Provide Feedback