Development and scripting FAQs
How do I develop scripts in FactoryTalk Optix Studio? What languages are
supported?
You can develop NetLogic scripts in C# with the use of FactoryTalk Optix Studio and
an external code editor to extend the functionalities of your FactoryTalk Optix
projects. See Extending projects.
Are there any NetLogic script examples available?
Yes, there are NetLogic script examples. See NetLogic tutorial.
Can I use external packages in my NetLogic scripts?
Yes, you can use external NuGet® packages in your NetLogic scripts. See NuGet packages.
To work with a specific firmware do I have to use a particular FactoryTalk Optix
version?
For firmware 6, you must use FactoryTalk Optix version 1.5 or greater.
Can I develop responsive UI with FactoryTalk Optix?
Yes, you can develop responsive UI with FactoryTalk Optix Studio. See Responsive user interface.
Where can I find and download FactoryTalk Optix application examples?
You can find and download FactoryTalk Optix Application examples in the FactoryTalk
Optix Help. See Application examples. You can also find
examples on the FactoryTalk Hub
Resources
page.What are the available communication drivers in FactoryTalk Optix?
You can check and learn about the available communication drivers in FactoryTalk
Optix Help. See Communication drivers overview and Communication drivers.
Can I downgrade the firmware of an Optix Panel?
No, the only way to downgrade firmware of an Optix Panel is to perform a factory
reset of the panel.
Provide Feedback