NuGet packages

Some library widgets and scripts require specific NuGet packages to be installed.
For more information about NuGet, see What is NuGet and what does it do? | Microsoft Docs.
IMPORTANT:
FactoryTalk Optix Studio
supports only .NET libraries with the .NET Standard 8 destination framework. To debug
FactoryTalk Optix Applications
with
Visual Studio®
or
Visual Studio Code®
, install .NET SDK.
IMPORTANT:
Rockwell Automation
is not responsible for any third-party software, including but not limited to its performance, security, updates, or compatibility with our products. Any use of third-party software is at your own risk, and we do not provide support, warranties, or guarantees for such software. Users should refer to the respective third-party providers for assistance and licensing terms.
Install NuGet packages in the code editor of your choice. See Install NuGet packages in Visual Studio and Install NuGet packages in Visual Studio Code.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal