Configure version control

Configure version control in
FactoryTalk Optix Studio
to commit, push, and pull project changes.
  1. In the title bar, select
    FactoryTalk Optix Studio Options
    and then
    Version control
    .
  2. Under
    Version Control User Configuration
    , in
    User Name
    , enter your user name.
    TIP:
    User Name
    is the name that appears next to commits when you open
    View history
    for a project. View history also identifies your commits with an avatar that uses the first letter of your name. For more information, see Version history.
  3. In
    User Email
    , enter your email address.
  4. (optional) To push to and pull from remote repositories of supported version control providers, configure user identities. See Add a user identity and Remove a user identity.
  5. (optional) To synchronize the available remote repositories across different
    FactoryTalk Optix Studio
    instances, sign in to
    FactoryTalk Hub
    . See Synchronize remote projects list.
  6. Select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal