Read operation codes

For each reading operation of single or multiple tags, the controller generates an operation code that describes the operation result.
Code
Description
Good
The reading operation is successful
BadNoCommunication
The reading operation failed because of a timeout (for example, a connection timeout).
The timeout value is determined by the
Timeout
property of a
Communication station
object.
BadCommunicationError
The reading operation failed because the controller returned an error
BadConfigurationError
The reading operation failed because of a tag configuration error (for example, an invalid address)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal