Store read operation codes

Configure the logger to store the operation codes of reading on the controller in the database.
TIP: For more information about the read operation codes, see Read operation codes.
Prerequisites
  1. To store read operation codes
  2. In
    Project view
    , select a data logger object.
  3. In
    Properties
    , set
    Log operation code of each variable
    to
    True
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal