Configure a web browser
    Add a web browser object to display web content at runtime.
- InProject view, underUI, right-click a container and select .
- InProperties, inURL, enter the website address that you want to display at runtime.TIP: The address that you enter must start with the protocol. For example,https://rockwellautomation.com
- (optional) InIncognito mode, select either:- True. Web browser runs in the incognito mode and does not store cache.
- False. Web browser does not run in the incognito mode and stores cache. This mode applies only to the native presentation engine and does not apply to the web presentation engine.
 TIP: By default, a web browser object runs in the incognito mode. You can disable the incognito mode to embed progressive web apps (PWAs) into your project and then use the PWAs without the Internet access. Disabling the incognito mode works only in the native presentation engine.
- (optional) InCustom headers, enter headers to send extra information in an API call.Each header must follow this format:. Separate headers by entering them in multiple lines.header_property:header_proprty_valueheader_a:value_a header_b:value_b
web browser
web
browser
    
Provide Feedback