Add an address bar
    Add an address bar for the 
Web browser
 object.
     TIP: 
    The address that you enter must start with the protocol. For example, 
https://rockwellautomation.com
Prerequisites
- To add an address bar
- InProject view, create aWeb Browserobject.
- Create anEditable Labelobject.
- Create variable of String data type.For more information, see Variables.
- (optional) Determine the start page by entering a web address as the variable value.For example, enterhttps://www.rockwellautomation.com
- Create a dynamic link between theTextproperty of theEditable Labelobject and the variable.For more information about dynamic links, see Create dynamic links.
- Create a dynamic link between theURLproperty of theWeb Browserobject andEditable LabelTextproperty.For more information about dynamic links, see Create dynamic links.
address
    
Provide Feedback