Configure and FTP client

  1. Install stable versions of the following NuGet package: FluentFTP. See NuGet packages.
  2. Configure the required
    FTPClientLogic
    script parameters. See FTP Client configuration.
  3. Run the
    FTPClientLogic
    script.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal