Array (File)/Misc Instructions

The file/miscellaneous instructions operate on arrays of data.
Available Instructions
Ladder Diagram
Selecting Mode of Operation
For FAL and FSC instructions, the mode tells the controller how to distribute the array operation.
If you want to:
Select this mode:
operate on all of the specified elements in an array before continuing on to the next instruction
All Mode
distribute array operation over a number of scans
enter the number of elements to operate on per scan (1-2147483647)
Numerical Mode
manipulate one element of the array each time the rung-condition-in goes from false to true
Incremental Mode
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal