Subdevices management
A user must have VPN permissions on a device to add or delete subdevices, change their settings, and manage the services that they provide.
- In the, access the section.FactoryTalk® Remote Access™Manager
- Select a subdevice in the domain (left) pane.Two information panels appear on the right pane:
- The subdevice information pane includes itsIP address.
- TheServicespane shows a list with the subdevice services. You can add, edit or delete a service.NOTE: See Add a service to learn more on this subject.
- Once you select a subdevice, you can:
Provide Feedback
to remove a subdevice.