Add a subdevice
- In the, access the section.FactoryTalk® Remote Access™Manager
- In the domain left pane, select the primary device on which the subdevice is dependant.
- Next to the primary device, in its same line, select
. Alternatively, select the three dots at the top of the screen and select Add subdevice. - ACreate subdevicedialog window opens. Enter the subdeviceNameandIP address.NOTE: The subdevice IP address must be compatible with a subnet that is reachable by the remote device.
- SelectSave.
Provide Feedback