Enable and disable project Automatic Diagnostics

Automatic Diagnostics automatically sends device diagnostic condition updates to applications and client devices supported by
FactoryTalk Alarms and Events
. Automatic Diagnostics is enabled by default.
TIP:
Automatic Diagnostics is supported only on
CompactLogix
5380,
CompactLogix
5480,
ControlLogix
5580,
Compact GuardLogix
5380, and
GuardLogix
5580 controllers.
To Enable or disable Automatic Diagnostics:
  1. On the main menu, select
    Edit > Controller Properties
    .
  2. Select the
    Advanced
    tab.
  3. Select or clear the
    Enable Automatic Diagnostics
    check box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal