Module Properties dialog boxes

Use
Module Properties
dialog boxes to configure:
  • General
    tab properties - View the module
    Type
    and
    Vendor
    and configure the module
    Name
    ,
    Description
    ,
    Slot, Minor Revision
    , and
    Electronic Keying
    .
  • Connection
    tab properties - Configure the
    Requested Packet Interval (RPI)
    ,
    Inhibit Module
    , and
    Major Fault On Controller if Connection Fails While in Run Mode
    .
  • Module Info
    tab - View module
    Identification
    and
    Status
    information.
Module Properties
dialog box tabs vary based on the controller or module. Some other
Module Properties
tabs include:
  • Power
    tab properties
    - View
    Power Unit Type
    ,
    Voltage
    , and configure
    Power Structure Rating
    .
  • Associated Axes
    tab properties - Choose a
    Server Update Period
    and
    Associated Axes
    .
  • Configuration
    tab properties - Configure filter time for points.
  • Setup
    tab properties- Choose a
    Drive File
    and view and edit parameter and link data associated with the drive.
  • Points
    tab properties - Enable Change of State for points.
  • Fieldbus
    tab properties - Launch RSFieldbus Software and view status information for Foundation Fieldbus devices.
  • RSNetWorx
    tab properties - Use this tab to launch RSNetWorx for EtherNet/IP to view or edit the respective network, associate a EtherNet/IP project file with the respective module, and audit an EtherNet/IP network.
  • SERCOS Interface
    tab properties - Use the
    SERCOS Interface
    tab to set and display the SERCOS baud rate, update rate for the SERCOS ring, and fiber optic transmit power range for the SERCOS ring.
  • Backplane
    - View module backplane data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal