Apply a control style to a graphic object

Apply a control style to a specific graphic object instance or type. Control styles overwrite the global style.
Prerequisites
  • Configure a stylesheet to contain multiple styles for a given graphic object type. See Configure a style sheet.
    For example, add a custom style for switch objects.
  1. To apply a style to a graphic object
  2. In
    Project view
    , select a graphic object or a graphic object type.
    For example, select a button. Button objects come with multiple predefined control styles.
  3. In
    Properties
    , in
    Style
    , select the drop-down arrow after the value and select the style to apply.
    For example, select
    Accent
    .
The graphic object or graphic object type uses the selected control style.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal