Apply a global style to the project

Select a style sheet in which to display the
FactoryTalk Optix Application
at runtime.
TIP: To change style sheets at runtime, see Develop a combo box to pick styles.
Prerequisites
  1. To apply a global style to the project
  2. In
    Project view
    , select either
    NativePresentationEngine
    or
    WebPresentationEngine
    .
  3. In
    Properties
    , in
    Style sheet
    , selectthe style sheet to apply.
The project applies the
Global Style
properties from the selected style sheet.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal