Restore a project to a commit
Restore a previous version of a project.
TIP:
When you restore a commit, the project in the local
repository updates to include the contents of the selected commit. Restoring a commit
permanently deletes any commits that occurred after the restored commit.
- From the toolbar, select.
View history - Select a commit to restore the project to.
- SelectRestore.
Version history
closes and the open project includes the changes of the selected commit.restore project
Provide Feedback