Version history
Use
Version history
to view all of the changes in the project
that are committed to a repository.Version history interface

Item | Name | Description |
|---|---|---|
![]() | User initial | The first letter of the user that committed the change to the repository. |
![]() | Commit message and details | The commit with the description of the change, the date and time of the commit.
Select to select the commit
and view the changes in the commit. |
![]() | Local or remote repository indicator | Icon indicates which repository contains the commit. Local history Remote history |
![]() | Change details | Indicates a change in the commit from the previous version. Expand the object to
see the highlighted values that changed in the object. |
![]() | Filter | Select either All to display the entire contents of the
project, or Updates to displays only changes to the selected
commits. |
version history
view history
Provide Feedback


to select the commit
and view the changes in the commit.