Last updated 4/01/2021
| Anti-Virus Software (from Detailed Information page) | Name and version number of the anti-virus software which was on the machine at the time of the test. |
| CPR | Rockwell software release the Microsoft Patch is installed on. |
| Date Published | The date Rockwell published its recommendation for this MS Patch. |
| Date Released (from MS Patch Summary and Detailed Information page) | This is the date Microsoft released the MS Patch. |
| Microsoft Priority (Rating) | Rating that Microsoft gives each patch, visit Microsoft at https://www.microsoft.com/en-us/msrc/security-update-severity-rating-system to learn more about the rating system. |
| MS Knowledgebase | This is the Microsoft assigned Knowledge Base article ID link to the Microsoft Webpage containing information about this MS Patch. |
| MS Patch Description | This description is produced by Microsoft at the time the MS Patch is released. |
| MS Security Bulletin (Depricated) | This is the Microsoft assigned Security Bulletin article ID number link to the Microsoft Webpage containing information about this Security Bulletin. |
| Notes | Any additional information regarding this MS Patch qualification. |
| Products | A list of Rockwell products tested for this patch qualification. |
| Qualification ID | An internal number used to track all test activities related to this MS Patch qualifications. Any questions regarding this MS Patch qualification should include this number. |