Local connection
The Local Connection mode lets you access the nor accessing Internet.
Interactive Access
features by connecting to a Runtime on the same LAN, without logging onto the FactoryTalk®
Remote Access™
ManagerIn this way, you can access a device where the Runtime software is installed with a VNC
(Virtual Network Computing) functionality besides additional features. Indeed, it allows you
to access the device automation network through a local VPN connection during both the
machinery development and commissioning phases, while remaining connected to the IT
network.
The Local Connection mode is supported by: Windows OS Runtime,
OptixPanel™
, OptixEdge™
, Stratix® 4300
, Embedded Edge Compute module.
NOTE:
To establish a Local Connection, follow the procedures below and
access System Manager as required.
To learn more about System Manager, download this user
manual:
You can also set up any other connection type from the connections available in the section.
NOTE:
See Interactive Access
for further information on this subject.
Manage local devices information
Once you have set up your devices, you can later manage the device information by using the
following settings:
- Remember password: Save your password. The newly saved password overwrites the old device password.
- Manage local devices: Select this option to add or delete a device, edit any existing device information or view a list of the saved devices and their related details, such as the devices name and IP address/host name.If you add a new device, complete the device name, IP address/host name and password.
NOTE:
Any entered IP address/host name is saved upon device connection.
In the Local Connection pane, if you check
Target device
before
completing the device information, only the IP adress/host name is saved. To save the
device name, enter the device name in the related field before checking
Remember password
.
WARNING:
Do not click on the password masked by bullet
characters to avoid it being cleared.
Local connection through Windows Runtime
To establish a Local Connection, proceed as follows:
- Start Windows Runtime.
- In the Windows Runtime pane, select theLocaltab and flag theEnable local connectionentry.
- Set a password to allow for later connection from your local device.
- Access theFactoryTalk Remote Access Tools Local Connectionfrom your local device..NOTE: TheFactoryTalk Remote Access Tools Local Connectionis automatically installed onto your device, when theTools are installed. See Tools to learn more about how to download the Tools.FactoryTalk® Remote Access™
- A dialog box opens up. Enter the IP address or the device name and the password previously set in theTarget deviceandPasswordfields of the dialog box.
- You will be prompted to accept a certificate to establish a temporary o permanent secure connection.
- TheInteractive Accesswindow opens up.
Local connection through Stratix® 4300 Routers, OptixEdge™
and OptixPanel™
Stratix® 4300
Routers, OptixEdge™
and OptixPanel™To establish a Local Connection, proceed as follows:
- Access the System Manager and selectFT Remote Accessfrom the main menu on the left.
- In theLocal Connectionsection, flag theEnabledentry.
- In the same section, set a password to allow for later connection from your local device. Click on theApplybutton.
- Access theFactoryTalk Remote Access Tools Local Connectionfrom your local device..NOTE: TheFactoryTalk Remote Access Tools Local Connectionis automatically installed onto your device, when theTools are installed. See Tools to learn more about how to download the Tools.FactoryTalk® Remote Access™
- A dialog box opens up. Enter the IP address or the device name and the password previously set in theTarget deviceandPasswordfields of the dialog box.
- You will be prompted to accept a certificate to establish a temporary o permanent secure connection.
- TheInteractive Accesswindow opens up.
Ensure connectivity despite IP address changes
The Local Connection Tool may encounter issues establishing a connection with a device if the device IP address changes after it has been registered. This can disrupt communication and lead to connectivity problems.
However, by saving the device host name instead of its IP address, you can mitigate this
issue. If you save the device hostname, the Local Connection Tool can query the DNS server
to resolve the hostname to its current IP address. This dynamic resolution ensures that the
tool can always find the device, even if its IP address changes.
This approach leverages the DNS server ability to translate hostnames into their corresponding IP addresses, maintaining a stable connection regardless of any IP address changes.
Provide Feedback