Interactive Access
The
Interactive Access
Tool is split into six sections:- Remote Desktop
- Processes
- Explorer
- Connection
- Information
- Log
You can access the in two ways:
or
Interactive Access
Tool through
the FactoryTalk®
Remote Access™
Manager- Access theand make sure that the device that you wish to control remotely is connected to a network.FactoryTalk® Remote Access™ManagerNOTE: See Runtime registration for further information on this subject.
- Select .
- Select the .NOTE: You might be required to authenticate to theInteractive AccessTool prior to continuing with the device registration.
NOTE:
Once you have selected
Tools
, click on your selection again to
proceed with the access.
NOTE:
When clicking on
Interactive Access
, a dialog window will show
up asking for permission to open the Interactive Access
Tool. Prior
to confirming, flag the Always allow
checkbox to prevent this
message from prompting again during this session. If you use a different computer or a
different browser, this message will prompt again.- Open theInteractive AccessTool by double-clicking on a device in the domain pane.
Provide Feedback