Summary of changes
This publication contains the following new or updated information.
Topic | Location |
|---|---|
Additional information to the Runtime entitlements description | |
Updated software options for OptixPanel devices | |
Added information on running a FactoryTalk® Optix™ application in a Docket container | |
Updated the Multifactor Authentication section | |
Added supports libraries that ease application development with predefined faceplates, devices, and objects. |
Provide Feedback