Discover how advanced wireless technologies are transforming industry. Private 5G and Wi-Fi are providing faster, more reliable, more secure connectivity, enhancing productivity, efficiency, and innovation. Rockwell Automation has been at the forefront, collaborating with our technology partners Cisco, Ericsson, and Nokia since 2019 to enhance product performance.
Industrial advanced wireless is transforming manufacturing
In our two-part webinar series we explore how Advanced Wireless solutions, like Wi-Fi and 5G Cellular, are expanding the industrial landscape, how next generation networking products are accelerating digital transformation and why the network is critical to the building resiliency in control system’s operation.
- Part One: Enable challenging industrial operations with Private 5G
- Part Two: Wi-Fi and Cellular (5G) Technology To Meet Plant Floor Needs
Create agile, resilient and sustainable industrial operations
5G: Edge-to-Cloud
- Provide low-latency connectivity, enabling real-time data transmission between edge devices and the cloud.
- Offer increased bandwidth and capacity, allowing for seamless scaling of edge-to-cloud deployments.
- Provide higher levels of reliability and network resilience, reducing downtime and improving service availability.
- Edge-to-cloud connectivity with 5G allows businesses to implement robust security measures at both the edge and the cloud.
5G: The Connected Worker
- Provide high-speed, low-latency, and reliable connectivity for AR/VR devices and applications.
- The combination of 5G with AR and VR enables immersive and interactive training experiences for workers.
- 5G enables connected workers to view dashboards, analytics, digital twins, and other FactoryTalk-based solutions on a tablet or smartphone in real-time.
- Technicians can access digital overlays, instructions, real-time data and connect with experts for real-time support while performing maintenance and repairs.
- Connected workers can view live video feeds from remote locations and overlay digital annotations, checklists, or guidelines onto their view for additional context to their tasks.
5G: Untethered Stationary Assets
- Private 5G networks provide high-speed, low-latency, fast roaming and reliable connectivity, helping to enable seamless operation of AGVs and AMRs in complex industrial environments.
- By using dedicated wireless spectrum and optimizing bandwidth usage among applications, private 5G network provides uninterrupted and prioritized connectivity to AGVs and AMRs.
- Private 5G networks offer increased capacity and coverage to support a many AGVs and AMRs simultaneously in a large geographical area.
5G: Mobile Assets
- Private 5G networks provide high-speed, low-latency, fast roaming and reliable connectivity, helping to enable seamless operation of AGVs and AMRs in complex industrial environments.
- By using dedicated wireless spectrum and optimizing bandwidth usage among applications, private 5G network provides uninterrupted and prioritized connectivity to AGVs and AMRs.
- Private 5G networks offer increased capacity and coverage to support a many AGVs and AMRs simultaneously in a large geographical area.
Explore the future of industrial connectivity with our Connected Enterprise Lab
We're investing in an advanced wireless lab to support our customers who might lack the resources to develop their own. This initiative will allow for Proof of Concept with our customers to test potential designs before trying to implement on the floor, helping to ensure the products we bring to market are fully functional and effective.
We are focused on general network wireless connectivity with both Private 5G cellular and Wi-Fi. We are testing specific OT use cases and understanding the design expectations of IT. We will be testing with OTTO 100AMR, ASEM 6300B and 6300PA, alongside several partner products.
System testing
- Bandwidth testing
- Time synchronization
- Roaming / radio handoff
- Latency
- Jitter
- QoS
Services
- Installation
- Site survey
- System design
- System testing
- Application testing
- System management
EtherNet/IP Testing on Private 5G
Rockwell Automation is testing our industrial automation products on Private 5G in our Connected Enterprise Lab.
R15 CBRS Testing Final Results
Tests were run according to a well-established Rockwell Automation test plan provided with strict success criteria of zero connection faults over a limited test period. The test plan included a series of test cases to establish reliable EtherNet/IP standard and safety (CIP Safety™) I/O connections from the GuardLogix® (used for monitoring test bed telemetry only, with various requested packet interval (RPI) settings, over the 5G core and RAN to the FLEX™ 5000 I/O standard and safety I/O in the test cases. The RPI is the period during which the controller and the distributed I/O modules exchange data.
Test Case | CIP Protocol | Test Description | RPI (Packet Interval) | Result |
---|---|---|---|---|
RA.CEL.1.1 | CIP I/O | Performance at 20 ms RPI | 20 ms | Pass |
RA.CEL.1.1 | CIP I/O | Performance at 5 ms RPI | 5 ms | Pass |
RA.CEL.1.3 | CIP I/O | Minimum Supported RPI | 0.5 ms | Pass |
RA.CEL.2.1 | CIP Safety | Performance at 5094 Default 20 ms RPI | 20 ms | Pass |
RA.CEL.3.1 | I/O + Safety | Concurrent Traffic Using Default (20 ms) RPIs | 20 ms / 20 ms (I/O, Safety) | Pass |
Learn more about industrial advanced wireless
Together we are making industrial advanced wireless a reality
We are partnering with our technology partners to provide private LTE, 5G and Wi-Fi technology for our customers.
System Integrator Partners
Rockwell Automation is working with System Integrators to help customers integrate Advanced Wireless technology to their manufacturing.
Others also viewed
Based on your activity